cancel
Showing results for 
Search instead for 
Did you mean: 

STD10P10F6

senda
Visitor

Edit By ST Moderator: Title of this post has been translated from Japanese to comply with the ST Community guidelines.

STD10P10F6 I would like to ask a question about the following.

Do you have documentation showing the location of this component in relation to the land relative to the external shape of the component?

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @senda, to the community!

This information is internal and not public. If you have a large business case, you are welcome to contact your local distributor or sales office.

However, if it is sufficient for you, you can draw diagonals across the corners of the moulding and obtain the centre of the chip quite accurately. The chip itself is about 30% of both the width and height of the moulding.

Hope that helps?

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.