cancel
Showing results for 
Search instead for 
Did you mean: 

st72F521 checksum problem

julien239955_stm1_st
Associate II
Posted on June 14, 2007 at 07:36

st72F521 checksum problem

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
julien239955_stm1_st
Associate II
Posted on June 12, 2007 at 12:31

Hi,

I'm in front of a problem by the using of a function which should give the checksum of my software.

#ifdef USE_HDFLASH_CHECKSUM

/*-----------------------------------------------------------------------------

ROUTINE NAME : HDFlashChecksum

INPUT : Flash address, Frequency

OUTPUT : Embedded Command Status

Returned values of Checksum are in EMBLG_PARAM_ENDH and

EMBLG_PARAM_ENDL addresses

DESCRIPTION : Compute a Checksum

-----------------------------------------------------------------------------*/

unsigned char HDFlashChecksum(unsigned char *Flash, unsigned char Freq)

{

EMBLG_PARAM_ECMD = 0x06;

EMBLG_PARAM_PTRL = ((int)Flash & 0xFF); // Flash Address Low Byte

EMBLG_PARAM_PTRH = ((int)Flash >> 8); // Flash Address High Byte

EMBLG_PARAM_FREQ = Freq;

FCSR = 0x00; // Launch command (no need to wait end of operation)

return EMBLG_PARAM_ECMD; // Return Embedded Command Status

}

#endif

How can I know the ''Flash Address Low Byte'' of my soft? So what should be the value of ''Flash''?

thanks for your help

wolfgang2399
Associate II
Posted on June 14, 2007 at 07:36

Hi,

although I don't really comprehend your problem in detail, I'll try to give some ideas.

Declaring the EMBLG_PARAM_PTR as pointer to an unsigned character with

char *EMBLG_PARAM_PTR;

you'll get the two byte number EMBLG_PARAM_PTR as pointer to an unsigned char.

To calculate the checksum you only have to add all the values of your flash from the first to the last byte.

checksum = 0;

 

for(EMBLG_PARAM_PTR = FLASH_FIRST_BYTE; EMBLG_PARAM_PTR <= FLASH_LAST_BYTE;) checksum += *(EMBLG_PARAM_PTR++);

where FLASH_FIRST_BYTE and FLASH_LAST_BYTE are constant pointers to the first and to the last byte of your flash.

But pay attention: If FLASH_LAST_BYTE == 0xFFFF you'll meet a serious problem: Increasing EMBLG_PARAM_PTR (== 0xFFFF) causes an overrun to 0x0000. Then the query EMBLG_PARAM_PTR <= FLASH_LAST_BYTE will give a wrong result and you might enter a deadloop!!!

In this case better use

checksum = 0;

 

for(EMBLG_PARAM_PTR = FLASH_LAST_BYTE; EMBLG_PARAM_PTR >= FLASH_FIRST_BYTE;) checksum += *(EMBLG_PARAM_PTR--);

Alternatively to declared constants you might take numerical constants as addresses:

checksum = 0;

 

for(EMBLG_PARAM_PTR = (unsigned char*)0xFFFF; EMBLG_PARAM_PTR >= (unsigned char*)0x8000;) checksum += *(EMBLG_PARAM_PTR--);

Hope it will help you to find a solution,

WoRo