2003-08-21 12:18 AM
2003-07-08 4:59 AM
When first powered on, my HDS2 starts in the run state - if I'm lucky it stops after 5-15 minutes and then RIDE or WGDB6 can communicate with it...
Does anyone have any idea why ?? Allenby2003-08-19 2:12 AM
Hello,
Try to power up the EMU before connecting the parralele LPT cable...perhaps your PC is introducing power through this cable and it disturbs the whole internal reset of the EMU.2003-08-21 12:18 AM
The emulator starts in run mode if the clock source is a signal input on the probe board (OSCIN position).This problem can get removed by two ways:
1.by giving power to the probe board.The probe board gets power when we connect application board and give it power. 2.by removing IC (74HC04) from the probe board.