cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F269 problem

poolsawat03
Associate II
Posted on October 11, 2007 at 08:30

ST10F269 problem

This discussion is locked. Please start a new topic to ask your question.
12 REPLIES 12
najoua
Associate II
Posted on October 01, 2007 at 08:36

/***********************************************************************/

Hello Sagai,

This is an example:

----------------------

/* */

/* SERIAL2 */

// Initialize the Asynchronous Serial Communication interface ASC0 to

// transmit a string at 9600 Baud, 8 Data and 1 Stopbit no Parity

//

// Use an interrupt to load the ASC0 Transmit Buffer Register

// Use your system terminal program to display the message.

/***********************************************************************/

#include

/********************************************************************/

sfrbit DP20 _atbit(DP2,0);

sfrbit DP21 _atbit(DP2,1);

sfrbit DP22 _atbit(DP2,2);

sfrbit DP23 _atbit(DP2,3);

sfrbit DP310 _atbit(DP3,10);

sfrbit P310 _atbit(P3,10);

/********************************************************************/

void init_sci_ch0( void );

void delay( void );

/********************************************************************/

#pragma global

static volatile char msg[] =

{

''Hello World, this is ST10F276 but soon it will be ST10F29x''

};

/********************************************************************/

void init_sci_ch0( void )

{

/* Port P3.10 = Serial Output, the TX pin */

/* first set port, before changing the direction (avoid glitch) */

_putbit (1, P3, 10);

DP310 = 0x01;

/* Asynchron mode, transmission only, no Error Checks */

S0CON = 0x0001;

/* 9600 baud the CPU clock frequency is 40MHz */

S0BG = 0x81;

/* Transmit Interrupt, ILVL=8, GLVL=0 */

S0TIC = 0x60;

/* Baud Rate Generator Start */

S0R = 1;

}

/********************************************************************/

// Serial transmit interrupt service routine

interrupt( 0x2A ) void s0_tx_int( void )

{

static volatile char *cptr;

static volatile char n=0;

static volatile char m=0;

if( n==0 )

cptr = msg;

m = *cptr;

if( m != '\0' )

{

S0TBUF = m;

cptr++;

}

else

{

n = 0;

return;

}

n++;

/* LEDs Games */

if(P2++ > 4)

{

delay();

P2 = 4;

}

}

/********************************************************************/

void delay( void )

{

volatile unsigned int t1, t2, t3=0;

for( t1= 15000; t1 > 0; t1-- )

{

for( t2=0xffff; t2>0; t2++ )

t3++;

}

}

/********************************************************************/

main()

{

volatile unsigned int p=0;

/* P2.0 - 2.3 = output */

DP20 = DP21 = DP22 = DP23 = 0x01;

/* LEDs = OFF */

P2 = 0xFF;

delay();

// init ASC0

init_sci_ch0();

/* Global Interrupt Enable */

IEN = 1;

/* Trigger Serial Transmission */

S0TIR = 1;

while( 1 )

{

/* LEDs Games */

if(P2++ > 4)

{

delay();

P2 = 1;

}

delay();

/* Repeat Transmission after delay */

if( p++ > 50 )

{

S0TIR=01;

p=0;

}

}

}

/********************************************************************/

Regards,

Najoua.

poolsawat03
Associate II
Posted on October 03, 2007 at 09:13

Hello Sir,

Thank you sir for your reply.

If want to change application from the ST10F269 to the ST10F276 and use only IFLASH , Is posible?

Do I need to initialize any other registers?

Could please help me on this?

Thanks and Best Regards,

sagi

najoua
Associate II
Posted on October 11, 2007 at 08:30

Hello Sagai,

Yes, it is possible to port your application from the ST10F269 to the ST10F276.

Please have a look to the AN2555 'porting an application from the ST10F269 to the ST10F276' available on the following link:

http://www.st.com/stonline/products/literature/an/13582.pdf

Best regards,

Najoua.