2009-08-21 6:11 AM
ST10 Flasher interface & Connection.
#st10-dump2009-01-19 5:52 AM
I have tried the 2nd MCU on this ECU, but all the same. Maybe it's require another software protocol which can start from the 0x86 responce?... Or not?...
Or there are any tricks to activate sBSL and read flash?...[ This message was edited by: gontsov on 20-01-2009 06:39 ]2009-08-21 6:11 AM
This interface can be used on other processors? example. St10f168-q, 272,280; automotive line? If so could i inform other models?
2010-07-06 12:21 PM
Of course, this tool can flash any ST10 due to the same init commands.
But it's can't dump the flash, even if port and monitor are fine:
*Dump-->ERROR Description: LoadExternalFlashMonitor: target Not found Only a writing of the hex-file is possible. Anybody knows how to start a flash dumping using this tool? Maybe it's just prohibited by ST policy or smth wrong there in the soft...