cancel
Showing results for 
Search instead for 
Did you mean: 

SPI Communiction

mailtoarup
Associate II
Posted on December 10, 2003 at 10:56

SPI Communiction

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
mailtoarup
Associate II
Posted on December 09, 2003 at 08:38

hello,

i want work on Interfacing AT93C46 EEPROM with my Microcontroller (ST72F264) on my softec demo board. using SPI protocol.I have connected :

PB7/SS pin to CS pin of AT93C46

PB6/SCK pin to SK pin

PB5/MISO pin to DO pin

PB4/MOSI pin to DI pin

VCC of AT93C46 is connected to 5v.

is it ok??/

In ST Application note AN970,diagram shows S pin of SPI EEPROM

is connected to one I/O pin of ST7.

and SS pin of ST7 is connected to VCC.

Now pls tell me what is the difference between theses two schemetics.

And tell me can i work on SPI ,the way i connected AT93C46 to ST7.

or pls suggest me how to connect AT93C46 to ST72F264..

As i m just learning pls tell me what all the issues i should consider in this application.I dont want use ST7 SPI internal register,instead want to write software code for communiction with eeprom

thanks,

Arup

jacktan1
Associate II
Posted on December 10, 2003 at 00:41

I cannot find the AN970. I think the 2 sch are both right.

You know, SPI com needs /SS, SCLK, SDO and SDI, the SPI controller in ST MCU can auto control these pins under correct setup. The /SS pin can be set to be a normal IO port , the /S signal can be output by a normal IO pin. You also can use 4 normal IO pins to simulate SPI.

J.V.
jatin
Associate II
Posted on December 10, 2003 at 10:56

Hello Arup,

You can control SS pin either using software or hardware. It can be done using the SSM bit in the SPICSR register. So, if you control the SS pin using software then your SS pin is free to use as normal I/O port.

lets say in your configuaration, you are connecting SS pin to the CS pin of the EEPROM. So in this case, you can select the micro in the master mode using software(bits SSM=1, SSI=1) and you are free to use the SS pin as normal I/O pin which is connected to CS pin.

For detailed info, please refer datsheet and App note (AN970).