cancel
Showing results for 
Search instead for 
Did you mean: 

Skip-jump table with Cosmic

henrik2
Associate II
Posted on July 06, 2007 at 07:38

Skip-jump table with Cosmic

This discussion is locked. Please start a new topic to ask your question.
7 REPLIES 7
henrik2
Associate II
Posted on July 03, 2007 at 14:25

Hi, I'm trying to make a skip-jump table for my IAP application. I have read all the previous threads here but still cant get it to work. Are there anyone who can support me with some code?

Regards

henke

luca239955_st
Associate III
Posted on July 04, 2007 at 06:38

Hello,

there's a code example in

http://www.stmcu.com/forums-cat-2946-1.html

Does it suit your needs?

Regards,

Luca (Cosmic)

henrik2
Associate II
Posted on July 04, 2007 at 06:44

Hi,

I have tried that code and I get error from compiler:

''redeclared external INT_jump_table''

Regards

Henke

luca239955_st
Associate III
Posted on July 04, 2007 at 14:57

that error is rather self-explanatory... are you sure you have put the different part of the example in the different source files as required?

Regards,

Luca

henrik2
Associate II
Posted on July 05, 2007 at 06:55

Hello Luca!

Oh, sorry. I see what you mean now. But I cant get it to work anyhow.

interrupt_vector.c:

-----------------------------

extern char INT_jump_table[];

char * const _vectab[] = {

INT_jump_table,

INT_jump_table+3,

INT_jump_table+6,

};

-----------------------------

jump_table.c

-----------------------------

#pragma section (INT_JMP)

char INT_jump_table()

{

#asm

xref _irq_trap;

jp _irq_trap

jp _irq_trap

jp _irq_trap

#endasm

}

#pragma section ()

@interrupt void irq_trap (void)

{

}

-----------------------------

Now I get this message from compiler:

''bad address (0x1000) for zero page symbol _INT_jump_table''

Thanks in advance, I really need your help on this...

Regards

Henke

luca239955_st
Associate III
Posted on July 05, 2007 at 13:10

send me your project at

mailto:luca.ubiali@cosmic.fr

and I'll take a look at it.

Regards,

luca

luca239955_st
Associate III
Posted on July 06, 2007 at 07:38

in case someone other than the OP was following this thread, the problem came from the fact that the memory model used put variables @tiny by default. The solution was to add @near in the line

extern @near char INT_jump_table[];

Luca