2024-01-31 12:34 AM
Two days ago, SDCC 4.4.0, a C compiler targeting various 8-bit architectures, including STM8, was released.
IMO, for the ST8, the main two improvements over SDCC 4.3.0 are:
For those who wonder how current C compilers for the STM8 compare, I've done a quick comparison:
http://www.colecovision.eu/stm8/compilers.shtml
Summary: SDCC is doing great, Cosmic is doing okay, the others not so much apart from very specific use cases (no surprise here - by now, IAR and Raisonance compilers haven't seen an update for years).
The official release for SDCC 4.4.0 is available in the SourceForge File release system:
https://sourceforge.net/projects/sdcc/files/
In addition to the source package, binaries are available for Windows, macOS, and GNU/Linux.
In addition to various bug fixes, notable features added since the 4.3.0 release are:
A full list of changes can be found in the ChangeLog:
https://sourceforge.net/p/sdcc/code/HEAD/tree/tags/sdcc-4.4.0/sdcc/ChangeLog
2024-01-31 1:46 AM
AIUI, the entire STM8 range is now NRND (Not Recommended for New Designs) ?
The 10-year "longevity" clock has already been ticking for a couple of years
2024-01-31 2:02 AM
It is also my understanding that the entire STM8 range is now NRND. IMO, that is very unfortunate - the STM8 makes a quite good target architecture for C compilers, and it was able to compete on price with many far less nice 8-bit architectures. AFAIK, the STM8 was also always cheap enough that no one even tried to fake them.
But ST apparently decided that being able to move some STM8 customers to STM32 was worth losing the rest of them.
SDCC is mostly a volunteer effort; as long as there are developers willing to maintain the stm8 port, SDCC will support the STM8. My guess it that we'll see at least another two decades of SDCC STM8 support.
2024-05-06 12:06 AM
Looks like STM8S, STM8L, STNRG, STLUX and STM8SPLNB are now "active", while STM8AF, STM8AL and STM8TL are still "NRND".
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.