cancel
Showing results for 
Search instead for 
Did you mean: 

Required microcontroller 8BIT 32KB FLASH 64QFP.

kat123
Associate
Hello ,

We need a microcontroller 8BIT 32KB FLASH 64QFP. we used MC68HC908AB32CFU that is NXP part now we want to go in STM microcontroller . Please suggest if which part is compatible with it.

Thanks and Regards Pooja Katariya

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
AA1
Senior III

I recommend STM8S207R6 (32KB) or STM8S207R8 (64KB), see: STM8S207/208.

Not likely to be anything close to pin or code compatible.

Why 8-bit?  Consider 32-bit STM32 Cortex-M0(+) type parts with more and current tool availability. Free Keil, free GNU based

Consider STM32C0 and STM32G0 families. Write in C, and port over application

What OTHER requirements do you need, size of FLASH perhaps doesn't directly correlate? Might indicate code complexity, 32-bit might do some operations more efficiently, good use of subroutines, and optimization can also help.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..