cancel
Showing results for 
Search instead for 
Did you mean: 

Real Time OS

e239955_stm1_stmicro
Associate II
Posted on February 09, 2005 at 17:43

Real Time OS

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
e239955_stm1_stmicro
Associate II
Posted on February 03, 2005 at 07:09

Is there anyone that has already and successfully an OS ported to STR71x target ?

If yes, what is the OS's name ? and what are the tools used ?

Thank you

gianfranco2
Associate II
Posted on February 03, 2005 at 07:34

Hi,

if i can add... RTOS with TCP/IP functionality...

hichem2
Associate II
Posted on February 03, 2005 at 11:25

Hello OneR,

We have already did this with a uClinux OS .

An application note,which describes how to port a uClinux on STR71x package, will be published soon.

Regard,

Hich :p

yu-jun
Associate II
Posted on February 03, 2005 at 23:19

We have already ported uC/OS-II to STR71x.

Our customer is using the OS for a STR710 application

e239955_stm1_stmicro
Associate II
Posted on February 04, 2005 at 04:45

Hi Zouh,

I'm really interested in your ucLinux port.

For the uc/Os II, is it an official port ?

Best regards

per239955_st
Associate II
Posted on February 04, 2005 at 07:02

Will these ports (uCLinux / uc/Os II) require any external RAM/ROM or will the internal memory be enough?

/Beach

sjo
Associate II
Posted on February 04, 2005 at 07:41

I have ported FreeRTOS to the str7, not a full rtos but small scheduler - ok for smaller 711/712 devices.

Regards

sjo

technischesoftware
Associate II
Posted on February 09, 2005 at 17:43

Hi sjo,

interested in the FreeRTOS port you made. Do you make it public ?

Regards,

CeeCee