cancel
Showing results for 
Search instead for 
Did you mean: 

Auto-reload timer

hfmarchesi
Associate II
Posted on February 10, 2005 at 06:56

Auto-reload timer

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
hfmarchesi
Associate II
Posted on February 09, 2005 at 07:22

How can i make a 50us timer using ST7LITE0? I'm using Indart-stx and the emulation is weird!!! Please help me!!!!!!!!!

wolfgang2399
Associate II
Posted on February 09, 2005 at 09:01

What do you want to do with the '50µs timer'?

Do you need one shot or periodical events?

What are you doing now and what is the result from the emulation in your application?

Please give more information!

WoRo

hfmarchesi
Associate II
Posted on February 09, 2005 at 09:30

I want to make a periodical sample. The microcontroller must generate an interrupt each 50us. In the emulation, the counters (CNTRH and CNTRL) don't count in a logical order and don't generate overflow. Therefore, the interrupt doesn't occur. I know that my doubt is basic but I'm new in ST Micro. :-] . Thank's for your help!!

wolfgang2399
Associate II
Posted on February 10, 2005 at 05:04

First an idea:

If you are using HiWare Compiler or assembler you have to take care to write first the MSByte (DCR0H) and then the LSByte (DCR0L) of the timer. Because writing to the DCR0H will disable the compare interrupt. Please see the notes on page 53 of the manual, even for further information.

Note: .... At reset, the counter starts counting from 0.

 

 

Caution: As soon as the DCR0H is written, the

 

compare function is disabled and will start only

 

when the DCR0L value is written.

 

If the DCR0H write occurs just before the compare event,

 

the signal on the PWM output may not be set to a low

 

level. In this case, the DCRx register should be updated

 

just after an OVF event. If the DCR and ATR

 

values are close, then the DCRx register shouldbe

 

updated just before an OVF event, in order not to

 

miss a compare event and to have the right signal

 

applied on the PWM output.

As 50µs is quite a short time, please have a look at the running-time of your interrupt routine.

Regards

WoRo

hfmarchesi
Associate II
Posted on February 10, 2005 at 06:56

I've worked more in my program, and tried follow your idea and it works. Many thank's!! :D