cancel
Showing results for 
Search instead for 
Did you mean: 

RAM debug macro files for JLINK and IAR compiler

fa
Associate II
Posted on November 09, 2005 at 07:02

RAM debug macro files for JLINK and IAR compiler

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
fa
Associate II
Posted on November 01, 2005 at 07:03

Does any one have a macro file, to enable RAM debug when using JLINK and IAR compiler?

Or is there another way to get RAM debug to work in IAR.

Best regards,

Frank Andersen

fa
Associate II
Posted on November 01, 2005 at 09:40

I have the IAR ver 4.30A, and a JLINK kicstart and kit with the STR711 from IAR. The problem is that all the examples are programmed into flash, if I select the configuration file to the Linker to xxxxx_ram.xcl, then the code is not excuted from RAM.

For the Atmel SAM7 there is a macro for Debugger, to be used when debuging in RAM, that is file I am looking for to the STR71x

Best Regards,

Frank Andersen

Posted on November 07, 2005 at 09:54

Hi,

I'm using winIDEA with IAR, but I think you should uncheck the flash loader box,

Manu

________________

Attachments :

iar.PNG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtOo&d=%2Fa%2F0X0000000aPT%2F7YLgQQsWEgqWPSY0t7LWT0iLhemmHIeLIQvBl90D_f0&asPdf=false