cancel
Showing results for 
Search instead for 
Did you mean: 

PSD Obj file.

happykkw
Associate II
Posted on February 25, 2005 at 07:08

PSD Obj file.

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
happykkw
Associate II
Posted on May 17, 2011 at 12:05

Hi all,

I got only a obj file(HEX format), and JCF file with uPSD 3233B. Can I get any PSD information from this Obj file? , such as ''Define PSD and MCU/DSP'', ''Pin/Node Functions'' ''Additional PSD Settings'' which defined in PSDExpress .

Thank you very much.

happykkw
Associate II
Posted on May 17, 2011 at 12:05

Thank you for reply!

Because I want to change the source and setting the PSD again, so I need to refer orgin PSD setting information. Do you have any suggestion to get the information from obj file, or other method?

I am just a PSD beginner, need help.

happykkw
Associate II
Posted on May 17, 2011 at 12:06

I mean that I don't have the ''ini'' which has original setting of PSD ,so I can not merge anything with HEX file, that is why I want to get that setting information from Obj file. I only have obj file, nothing else.

Thanks