cancel
Showing results for 
Search instead for 
Did you mean: 

Problems with the breakpoints in the debugger of the uVision2 & 3!!

miguell
Associate
Posted on February 28, 2008 at 12:24

Problems with the breakpoints in the debugger of the uVision2 & 3!!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
miguell
Associate
Posted on May 17, 2011 at 11:52

When I try to emulate a program with several banks with the debugger of uVsion, if I put a breakpoint in a code line of the any interrupt routine (link on common area), the debugger doesn't stop. The program is executed correctly.

Does somebody know which is the problem? Do I need configurate any parameter in the uVision?

Thanks for your help,

Miguel