2006-12-19 5:36 AM
2006-12-19 1:39 AM
Hi, I have not the administrator privilege on the PC where the Softec Microsystem ST7 toolset (v. 3.00 based on STVD 3.1.0) is installed.
When I try to open a workspace, the tool search for application file ''*.exe'' files instead of workspace file ''*.stw''. Choosing the option ''all files'' (*.*), the workspace is founf and opened, but the debug does not work. Entering with administrator privilege, there is not any problems.2006-12-19 5:36 AM
This is taken from the release notes for Visual Develop:
Administrator privileges are required to install STVD7 and to connect emulators to the USB port for the first time. Power user or administrator privileges are required to run STVD7. Regards sjo