cancel
Showing results for 
Search instead for 
Did you mean: 

Problem to read Flash Protection Register using Read Protection Sattus

y_gudekar
Associate II
Posted on March 20, 2006 at 13:40

Problem to read Flash Protection Register using Read Protection Sattus

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
y_gudekar
Associate II
Posted on March 20, 2006 at 13:40

Dear all,

We are able to achive functionality for, ''Read/Reset'', ''Program Word'', ''Block Erase'' and ''Chip Erase'' command for ST10F269.

But we are unlucky to achive functionality for ''Read Protection Status''.We are implementing this command as follow.

Read_Prot_Sts PROC

MOV R7,#00F0h ; Command Cycle 1 Of Read/Reset

EXTS R11,#01 ;Use EXTended Addressing for next MOV Instruction

MOV [R12],R7

MOV R5,#02a54h ; //Command Address

MOV R6,#015a8h ; //Command Address

SCXT dpp0,#08h

MOV R7,#00A8h ; Command Cycle 1

MOV [R5],R7

MOV R7,#0054h ; Command Cycle 2

MOV [R6],R7

MOV R7,#0090h ; Command Cycle 3

MOV [R5],R7

POP dpp0

MOV R13,[R12]

MOV R7,#00F0h ; Command Cycle 1 Of Read/Reset

EXTS R11,#01 ;Use EXTended Addressing for next MOV Instruction MOV [R12],R7 ;address id Don't care for Read/Reset Command

RET

Read_Prot_Sts ENDP

Is there any problem in above code? plz help us.

Thanks.....

Yogesh Gudekar.