2025-06-19 12:44 PM - last edited on 2025-06-20 12:45 AM by Peter BENSCH
Hi ST Community!
I'm working in a HV power design (400VDC) with a STPSC6H065DLF Schottky diode.
I can see from its datasheet that pins 1 and 2 are not connected internally, but I can't find any recommendation about what to do with those pins. Would it be safe to connect them to the Anode?
I'd like to attach a copper plane to them, for improving thermal disipation, but in the other hand I don't want to have a floating copper plane in that area, since it's a switching one.
Any recommendation or suggestion will be welcome.
Thanks in advance.
Julián Carrizo
Electronic Engineer
2025-06-20 12:55 AM
Welcome @jcarrizo, to the community!
Well, you are welcome to measure to be on the safe side, but there are only two ways in which the NC pins on this diode could be connected: either to the anode or to the cathode. If one of these were true, NC would not be Not Connected, but would be labelled with the respective connection. In addition, the NC pins would have to be bonded in order to connect them to the anode, which would only cause additional costs.
So the only conclusion that remains is that the NC pins are what they are labelled as: Not Connected.
Hope that answers your question?
Regards
/Peter
2025-06-20 3:06 AM
I don't think the question was about the internal connections ...
2025-06-20 3:57 AM
Well, the fact that there are no internal connections due to the lack of bonding means that you can connect the NC pins wherever you want. However, a connection from the NC pins to the cathode would significantly reduce the air and creepage distance and would therefore not be a good idea.