2023-10-06 4:20 AM - last edited on 2024-07-08 7:00 AM by Peter BENSCH
Dear Technical Support,
Could you provide me the MTBF of ATECC608A-MAHDA-T and the temperature which it was determined and the energy activation value?
Thank you so much,
María
Solved! Go to Solution.
2023-10-06 4:44 AM
Welcome @MariaMTBF, to the community!
I would be more than happy to help you with this question. However, this possibility is denied to me because ATECC608A-MAHDA-T has nothing to do with STMicroelectronics and is produced and supported by another manufacturer.
If the problem is solved, although perhaps not to your complete satisfaction, please click Accept as Solution. This will help other users find that answer faster.
Good luck and kind regards
/Peter
2023-10-06 4:44 AM
Welcome @MariaMTBF, to the community!
I would be more than happy to help you with this question. However, this possibility is denied to me because ATECC608A-MAHDA-T has nothing to do with STMicroelectronics and is produced and supported by another manufacturer.
If the problem is solved, although perhaps not to your complete satisfaction, please click Accept as Solution. This will help other users find that answer faster.
Good luck and kind regards
/Peter
2023-10-08 11:45 PM
Ups! Sorry, Peter. Thank you so much for your reply!!!
Could you help me for knowing the MTBF of LSM6DSV16XTR? The temperature which it was determined and the energy activation value?
Best regards,
María
2023-10-15 11:47 PM
Since it is a different component than the one mentioned at the beginning of the thread, I would like you to create a new thread for it. Alternatively (not in parallel please) you can also create a personal ticket at the Online Support System OLS.
Good luck!
/Peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.