cancel
Showing results for 
Search instead for 
Did you mean: 

LCD resolution

sriharsha
Associate
Posted on March 11, 2014 at 13:29

Hello,

Might be a silly question, but I want to know how can we get an idea of display pixel resolution when the specs say the lcd controller capability is 40*8 segments or so?

Regards,

Harsha

#lcd #controller #resolution
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Posted on March 12, 2014 at 21:34

You need to be careful here, LCD can means something other than a pixel addressable panel, when it dealing with elements it's probably an

http://www.dkedisplay.com/product_search/lcd_glasses.htm

, like on a watch, thermostat.

For graphics you probably want a pixel addressable panel, with an LCD controller, and screen buffer, and which attaches on a 8/16-bit external memory bus (EBI/FSMC)

There are also text/character based displays what might have 5x7 fonts, and 20x4 or 16x2 character displays, these typically use a 4/8-bit data interface and address line for control/data, and can be interfaced to micro-controllers via some GPIO

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..