cancel
Showing results for 
Search instead for 
Did you mean: 

Is the MOSFET (STP85NF55L) reliability affected if the Vgs is near to the maximum specified in the datasheet?

IGent.1
Associate

My customer specifies a relation of 60% of the maximum Vgs for operation. My design is using 80% of the maximum Vgs. They are asking how this increase will affect the component reliability (failure mechanism, failure rate...).

My design is eqquiped with 4 STP85NF55L, operating at 32Hz (PWM) resistive loads.

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0