cancel
Showing results for 
Search instead for 
Did you mean: 

INDART + USB

shermantec
Associate II
Posted on August 04, 2003 at 10:15

INDART + USB

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
shermantec
Associate II
Posted on August 03, 2003 at 11:53

Hello

In the Softecmicro - Indart program there is an option for Emulator , I want use it but there is only 2 options -> LPT1 and 2 .

Where is the USB ?

Latino
ppoletto
Associate II
Posted on August 04, 2003 at 06:03

What kind of inDART model do you have? The code is placed in the board.

For inDART based on USB communication, no port settings are required. You have only to select the correct hardware model code in the communication Settings dialog box.

--Piero
shermantec
Associate II
Posted on August 04, 2003 at 06:56

Hello

I intall the Softec Indart for the ST7lite and the OS ask me for a driver for the USB and i don't have it .

Where i can find it ?

Latino
pxausa
Associate II
Posted on August 04, 2003 at 10:15

You must first install the software, and THEN plug the inDART unit to the PC. Windows will automatically recognize the instrument.