cancel
Showing results for 
Search instead for 
Did you mean: 

Im searching for a replacement of the ST62T65C6

RRODR.1
Associate II

My aplication is cpu to coffee machine professional...

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

As Tesla said, there is in fact no replacement for such an old microcontroller, which was discontinued many years ago. Since then, there have been an extremely large number of further developments, so that a change to a newer platform is imperative.

However, with STM8, one should not rely on a family that is not significantly younger than the ST6 and will not be available in the foreseeable future. Instead, more modern mcu such as the STM32G030K6 or STM32G031K4 would be recommended, which can easily cover the functions of the plain old ST6.

If EEPROM is necessary, one could also take a look at the STM32L010K4 because of its EEPROM technology, but due to the current extremely high demand, it is probably better to use an STM32G0 and emulate EEPROM in flash there.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

6 REPLIES 6

>>My application is cpu to coffee machine professional...

For people who are outside the coffee machine design engineering field, what are the actual requirements?

What functionality does the existing MCU implement? Do you have any of the design documents or source with which to gauge the complexity, functionality, and number of interfaces it drives or senses?

Perhaps something in the STM8 family?

Not something massively complex, with low cost, and availability?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..

Thank you very much for your kindness. We have pulse readings, timers, temperature controls and common triggers for motors and valves. They are equipment that are in use on the market and not a new project. Thank you one more time. Let's check out the STM8 family.

>>..not a new project. 

Sure but you're likely going to have to redesign a sub-section of the board to accommodate new parts to get equivalent functionality, there's not going to be a drop in replacement.

If a 28-pin DIP might be able to replicate with a module level implementation using modern SMT parts.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Peter BENSCH
ST Employee

As Tesla said, there is in fact no replacement for such an old microcontroller, which was discontinued many years ago. Since then, there have been an extremely large number of further developments, so that a change to a newer platform is imperative.

However, with STM8, one should not rely on a family that is not significantly younger than the ST6 and will not be available in the foreseeable future. Instead, more modern mcu such as the STM32G030K6 or STM32G031K4 would be recommended, which can easily cover the functions of the plain old ST6.

If EEPROM is necessary, one could also take a look at the STM32L010K4 because of its EEPROM technology, but due to the current extremely high demand, it is probably better to use an STM32G0 and emulate EEPROM in flash there.

Good luck!

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

If the problem is resolved, please mark this topic as answered by selecting Select as best under your preferred answer. This will help other users find that answer faster.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RRODR.1
Associate II

Thank you very much, we have an excellent solution. We're working on it. Thank you so much for your dedication and kindness.

Roger