2007-05-17 6:52 PM
If jtag send message like cannot stop the cpu
2011-05-17 12:43 AM
This post is intended to help everyone who got message from jtag
like ''cannot stop the cpu'' Yesterday i restored the CPU(that was in 'hanging' state) I choosed the option for jtag ''Use reset at start up'' , but this not helped. The problem was that we need Global reset at start up because in my case 'hanging' was caused by playng with FMI register. This may be done if you create circuit that tern on power simultaneously with start of jtag(or to use the reset signal from jtag to tern on the power).