2006-08-28 5:57 AM
2006-08-25 8:24 AM
I will be using the ARM RealView Developer Suite, which my company has already purchased, to develop firmware for the STR711
Can anyone help me find a cheap JTAG ICE for that will work with the ARM RealView tools? I would prefer a USB interface to ICE. I thought that maybe the ICE that comes with the STR-RVICE/ME might work, but I am having a lot of trouble trying to buy one. I have been using the IAR jLink that came with an STR711 eval board. This worked great, but the compiler is limited to 32K and my company won't pay for the full version.2006-08-28 5:57 AM
ARM is quoting about US$3000 for either one which is more than I want to spend. Will the ICE that comes with the STR-RVICE/ME work with the full version of the ARM Realview suite? It seems like it would, but I am having a hard time getting a straight answer from ARM or ST. I know the STR-RVICE/ME is limited to ST chips, but that's OK with me. It's only about $300.
Jeff