cancel
Showing results for 
Search instead for 
Did you mean: 

IAP

asherman
Associate II
Posted on April 02, 2003 at 13:50

IAP

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
asherman
Associate II
Posted on May 17, 2011 at 11:33

Can we make IAP on the ST92F150 with the RS232 ?

johanpauvert2
Associate II
Posted on May 17, 2011 at 11:33

Yes. Using RS232 or other serial communication (CAN, SCI etc.).

The AN1275 (In-Application Programming for the ST92F120) has the drivers you are looking for : updating the Flash and EEPROM

memory by receiving a standard Intel® hex file via a RS-232.

It can be easily ported to the ST92F150.

Other useful links :

- AN977 : Guidelines for upgrading from the ST92F120 (0.50 ¦m) to the ST92F124/F150/F250 (0.35 ¦m)

- ''Simple program example?'' discussion from the ST9 forum

Ciao

Skywalker
asherman
Associate II
Posted on May 17, 2011 at 11:33

Is there an option to make IAP with the I2C ?

johanpauvert2
Associate II
Posted on May 17, 2011 at 11:33

You can use any communication protocol and this includes I2C.

Just replace the communication drivers in AN1275 by the I2C ones.

FYI, I2C drivers can be found the ''ST9+ I2C'' discussion. With or without DMA access.

Skywalker