2003-10-08 2:44 PM
IAP _ Trying to write a byte into the main flash while exec form boot flash
2011-05-17 2:55 AM
Hi
I need help. Just got the DK3200 kit. I got both com running using int. Timer... I am trying to write a byte to the main flash the mapping is: 8000 FFFF _ exactly the same as the one on AN1560 VM = 0x86 FLASH_COMMON_XAAA (volatile unsigned char xdata *) 0x9AAA FLASH_COMMON_X555 (volatile unsigned char xdata *) 0x9555 FLASH_BOOT_XAAA (volatile unsigned char xdata *) 0x0AAA FLASH_BOOT_X555 (volatile unsigned char xdata *) 0x0555 I am running the code from the second flash ( program only). the function to write byte is from from the second flash. the function to write byte is from flashcode1.c form the code of the usp demo code. I can't write into the flash. the function return but the byte remain unchanged 0xFF. To check this I read back by both my code and the upload from the PDSsoftexpress. Please help !!! _2011-05-17 2:55 AM
1 - Data read/write signals must be able to access the flash you intend to program, that means that your VM must be set to 0X96.
2 - Since the main flash is paged, set your page register to the flash that you want to access. 3 - All interrupts must be disabled to ensure proper timing of the flash read/write sequences. Good luck, Asterix2011-05-17 2:55 AM
Thanks
I got it now VM 0x96