cancel
Showing results for 
Search instead for 
Did you mean: 

I2C Problems

shermantec
Associate II
Posted on October 31, 2003 at 05:21

I2C Problems

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
shermantec
Associate II
Posted on October 29, 2003 at 14:38

After spending some days of unsuccessful experiments i need urgent help.

We use the I2C at Slave mode.

After receiving the Address match and the ADSL flag become '1'

Then, reading of the SR1, SR2, and DR to reset ADSL,

and here is the problem after ADSL flag is go to '0' , the BTF and TRA

become immediately '1', without any activity at the I2C bus.

The ways I found to reset them are: 1) writing to DR, 2)up and down the

STOP bit and 3)disable the I2C by take PE '0'.

Why do I get these flags at all?
peterharris9
Associate II
Posted on October 29, 2003 at 17:35

Hi Latino

My I2C interrupt service routine looks like this:

#pragma asm

sim; /* mask interrupts */

#pragma endasm

copy_of_I2CSR1 = I2CSR1;

copy_of_I2CDR = I2CDR;

copy_of_I2CSR2 = I2CSR2;

do your processing on the register copies here

#pragma asm

rim; /* unmask interrupts */

#pragma endasm

This routine works for both slave receive and master transmit.

Hope this helps

BM

april_t
Associate II
Posted on October 30, 2003 at 05:36

Hi BM

I have try the suggested sequence of commands and its stays the same.

after initialization, when the i2c bus send my address, the st7 identifies the match and take ADSL flag high.

Immediatly after i read the I2CST1, I2CDR and I2CST2 to copy of them, (as instructed)

Instead of make EVF & ADSL '0' and leave BUSY '1',

the st7 make ADSL '0' and EVF, BTF,BUSY, TRA '1' - of course this is incorrect because the I2C bus didn't recieve or transmit anything in 10 uS time !!

help please.....

sory about the long explanation but i try to make things clear.

regards

room
peterharris9
Associate II
Posted on October 30, 2003 at 17:28

Hi

It is strange that TRA == 1. This is saying that a byte has been transmitted.

If you are using interrupts rather than polling, make sure interrupts are masked while you are servicing them.

Here is my initialisation routine for the I2C port:

I2CCR = 0x00; // Force reset

I2COAR2 = 0x40; // Fcpu = 8MHz FXtal/2

I2CCCR = 0x26; // I2C clock rate = 100kHz

I2CCR = PE; // Enable port

I2CCR = PE|ENGC|ACK|ITE; // Config: port enabled, general call enabled, acknowledge enabled, interrupt enable

#pragma asm

rim; /* unmask interrupts */

#pragma endasm

april_t
Associate II
Posted on October 31, 2003 at 05:21

Hello BM

Thanks for the replay, But, ....

As I say at my previus note the incorrect signals in SR1 are apeared immediatly (whithin 3 to 10uS) )after I reset the ADSL.

So, the BTF and TRA aren't signaling for real I2C cycle that happend but it is an incorrect and faulty signals.

The some problem happend in interrupt mode and in polling mode I have tried both of them.

I use logic analyzer to watch the exact content & timming of signals of the I2C bus versus the SR1 register.

This phenomena is quiet stable for all my expriments of the previus week and yes, I tried to replace the chip to new one.

Help !!!!

thanks

room