2006-07-27 9:09 PM
2006-07-18 11:55 PM
Hello I am working on a byte read routine.
I want to read a single byte from the EEprom. I found this information in the datasheet for M24C32-: ''... The bus master must not acknowledge the byte, and terminates the transfer with a Stop condition.'' One of the examples of found her in the forum ''Byte read from the external I2C EEPROM mounted on the STR710 demo board'' has a function EEPROM_byte_read: /* Send the EEPROM address with LSB bit set */ I2C_AddressSend (I2C0, M24C08_Block0ADDRESS, I2C_Mode7, I2C_RX); while (I2C_FlagStatus (I2C0, DIRECT, I2C_ENDAD)==RESET); I2C_FlagClear (I2C0, I2C_ENDAD); /*Read 'Buffer_Size' bytes from the EEPROM starting from address 0x00 of Block0 and place them in Rx_Data[] array */ /* Generate STOP condition */ I2C_STOPGenerate (I2C0, ENABLE); /* Read byte */ I2C_Rx_byte = I2C_ByteReceive(I2C0); I would have expected something like I2C_AcknowledgeConfig. Other examples, that read more bytes had special cases for the second last byte and the last byte to receive. Did I get something wrong?2006-07-19 12:39 AM
I have changed the receive function:
TEepromData EepromByteRead(u16 address) { TEepromData data; u8 buffer[2]; I2C_Tx_Status status; u8 dummy; //Generate Start I2C_FlagClear (I2C1, I2C_ENDAD); I2C_STARTGenerate(I2C1, ENABLE); while (I2C_FlagStatus (I2C1,DIRECT,I2C_SB)==RESET); //Transmit the address as write mode I2C_AddressSend (I2C1,EEPROM_ADDR,I2C_Mode7,I2C_TX); //Test the end of address transmission while (I2C_FlagStatus (I2C1,DIRECT,I2C_ENDAD)==RESET); I2C_FlagClear (I2C1, I2C_ENDAD); //Transmit the address de memory buffer[0] = address >> 8; buffer[1] = address & 0xFF; status = I2C_BufferSend (I2C1, buffer,2); //Generate Start I2C_STARTGenerate(I2C1, ENABLE); while (I2C_FlagStatus (I2C1,DIRECT,I2C_SB )==RESET); //Transmit the address as read mode I2C_AddressSend (I2C1,EEPROM_ADDR,I2C_Mode7,I2C_RX); //Test the end of address transmission while (I2C_FlagStatus (I2C1,DIRECT,I2C_ENDAD)==RESET); I2C_FlagClear (I2C1, I2C_ENDAD); //Receive the data I2C_AcknowledgeConfig (I2C1, DISABLE); data = I2C_ByteReceive (I2C1); //Generate Stop I2C_STOPGenerate (I2C1, ENABLE); I2C_AcknowledgeConfig (I2C1, ENABLE); return data; } To the the function I have used this code: u8 i; i=0; while(i EepromByteRead(i); EepromByteRead gets stuck somewhere while looping. Sometimes I can read several bytes before it locks up, sometimes it locks up on the first loop. Locking up means the code ist stuck in the ''Generate start'' while loop: //Generate Start I2C_FlagClear (I2C1, I2C_ENDAD); I2C_STARTGenerate(I2C1, ENABLE); while (I2C_FlagStatus (I2C1,DIRECT,I2C_SB)==RESET); This has happened before (before I added the I2C_AcknowledgeConfig lines). Maybe we have to wait for a flag after generating STOP? Alexander Mueller littleBLUE GmbH2006-07-27 9:09 PM
I'm tryin to communicate with a TI DA5571 dac, but my application got stuck in the instruction
while (I2C_FlagStatus (I2C1,DIRECT,I2C_ENDAD)==RESET); I can't see nor the clock neither the address address data out of the micro pins. Any suggestions ? thanks in advance GM