2020-12-11 4:23 AM
2021-04-30 12:15 PM
Did you ever figure this out? I am looking at the same thing. Perhaps it is controlled only by the module when it goes into powerdown and is not able to be changed via a command?
2021-04-30 12:36 PM
Similar devices it relates to low power and power down modes, for example when put in a sleep or intermittent wake cycle.
Signal used to gate LNA or external antenna bias
2021-04-30 12:39 PM
Thanks for the super quick response!! So controlled by the module only, correct? Not able to be controlled via software command over UART?