cancel
Showing results for 
Search instead for 
Did you mean: 

How do use STVD7 Head files ???

hongluo
Associate II
Posted on October 21, 2004 at 09:42

How do use STVD7 Head files ???

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
hongluo
Associate II
Posted on October 21, 2004 at 07:11

Hello all:

I'm a beginner.

I want to use the head file in ''C:\Program Files\STMicroelectronics\st7toolset\include\ST72F324J6.h''.

But I don't know how do go to use,especial following code:

/* System Integrity Control/Status Register */

STVD7_EXTERN volatile unsigned char SICSR @0x2b;

define SICSR_WDGRF 0 /* Watchdog Reset Flag */

define SICSR_WDGRF_OR (1 << SICSR_WDGRF)

define SICSR_LVDRF 4 /* LVD Reset Flag */

define SICSR_LVDRF_OR (1 << SICSR_LVDRF)

define SICSR_AVDF 5 /* Voltage Detector Flag */

define SICSR_AVDF_OR (1 << SICSR_AVDF)

define SICSR_AVDIE 6 /* Voltage Detector Interrupt */

define SICSR_AVDIE_OR (1 << SICSR_AVDIE)

define SICSR_AVDS 7 /* Voltage Detection Selection */

define SICSR_AVDS_OR (1 << SICSR_AVDS)

could anybody help me,please?

alain2399
Associate II
Posted on October 21, 2004 at 09:42

Here is an example using the ADC of the ST7Lite09. I hope it is clear enough.

Best regards.

/* ---------------------- (c) 2003 STMicroelectronics ------------------- */

/*********************************************************/

/* This program uses the ST7FLITE09. It configures the ADC to convert on */

/* channel AIN1 (PB1), scales the value read on 4 bits and sends the result */

/* on PA0/1/2/3. */

/* With the simulator, use the ADC_Stimuli.in file as input stimuli and plot */

/* the AdcValue variable, PA0/1/2/3 and PB1 pins, run the simulator and */

/* visualize the results with the plotter. */

/****************************************************/

/* Include file provided by STVD7 describing the registers mapping. */

#define __DEFINE_REGISTERS_STVD7_INCLUDE__

#include

#undef __DEFINE_REGISTERS_STVD7_INCLUDE__

/* Define Macros for bit manipulation. */

#define SetBit(VAR,BIT_NUM) ( (VAR) |= (1<

#define ClrBit(VAR,BIT_NUM) ( (VAR) &= ((1<

#define ValBit(VAR,BIT_NUM) ( (VAR) & (1<

#define BitIsClear(VAR,BIT_NUM) ( 0 == ValBit(VAR,BIT_NUM) )

#define BitIsSet(VAR,BIT_NUM) ( !BitIsClear(VAR,BIT_NUM) )

/* Global variable */

unsigned char AdcValue;

/*******************************************************/

void main(void)

{

/* Configures port A0/1/2/3/4 as output. */

PADDR = 0x1F;

PAOR = 0x1F;

PADR = 0x00;

/* Enables the ADC on AIN1. */

ADCCSR = ( ADCCSR_ADON_OR | ADCCSR_CH0_OR );

while(1)

{

/* Waits for the end of the conversion. */

while(BitIsClear(ADCCSR, ADCCSR_EOC));

/* Reads the A/D value. */

AdcValue = ADCDR;

/* Divide it in order to have it on 5 bits */

/* and writes it on the PortA. */

PADR = AdcValue >> 3;

/*******************************/

}

}