cancel
Showing results for 
Search instead for 
Did you mean: 

Frequency of PWM: very un-precise!?

marcosarti29
Associate II
Posted on February 02, 2007 at 06:46

Frequency of PWM: very un-precise!?

This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
marcosarti29
Associate II
Posted on January 22, 2007 at 11:08

Hi,

I use ST7lite19F with internal oscillator at 8MHz.

I use initial re-calibration with:

MCCSR = 0x00;

EECSR = 0x00;

RCCR = ((EEPROM[0] & 0xFF00) >> 8);

I use PWM with clock at 32MHz:

ATCSR = 0x1A; /* fcounter = 32 MHz, OVFIE */

ATR = 2496;

With this setting my fPWM is fCOUNTER /(4096-2496) = 32MHz/1600 = 20KHz.

Problem: when I go to measure the real frequency I found variable value, 18KHz to 33KHz ??!!! :o

It's normal? :(

pjr
Associate II
Posted on January 24, 2007 at 12:26

To me this code:

RCCR = ((EEPROM[0] & 0xFF00) >> 8);

sets RCCR to 0. The eeprom holds bytes, so 8 bits of eedata & 0xFF00 = 0.

What are you setting the DCRx register(s) to?

pjr

marcosarti29
Associate II
Posted on January 29, 2007 at 06:04

Thanks for your reply!

Why RCCR is '0'?

The DCRx start to ATR and it's go at 4096 for slowly start.

Thanks

marcosarti29
Associate II
Posted on February 02, 2007 at 06:46

Perhaps I have found!

I have mapped the EEPROM:

MY_EEPROM = NO_INIT 0x1000 TO 0x107F;

with:

NV_VAR INTO MY_EEPROM;

and defined it in main.c :

#pragma DATA_SEG NV_VAR

RAM_EXTERN unsigned int far EEPROM[0x40];

When I read the EEPROM with the command:

MCCSR = 0x00;

EECSR = 0x00; /* E2 in lettura */

RCCR = ((EEPROM[0] & 0xFF00) >> 8);

is possible that I read the least bit of RCCR?

Thanks for help!