cancel
Showing results for 
Search instead for 
Did you mean: 

Flash Writing Problem

satnam
Associate II
Posted on July 30, 2009 at 11:48

Flash Writing Problem

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
satnam
Associate II
Posted on May 17, 2011 at 09:59

Dear All,

I are facing a problem while writing secondary flash, the time taken to write a single halfword is more then 500ms.

As per Eratta sheet(rev 5) for STR912FAw44 MCU, for writing to flash we need to set the bit 18 of configuration register of ARM core.

I have tried by writing the code given in eratta sheet

1. Before flash writing command, in this case the MCU takes more then 500 ms to write a single half word to flash. i.e. no change from earlier case.

2. After the flash writing command, in this case the MCU hangs as soon as the first halfword command is executed.

The code is pasted below.

Please help us, we need to reduce the time required the flash.

The scu clock for flash is also enable while initializing the MCU.

u8 Flash_Write_Word(u32 FlashSector,u32 Offset,u16 *DataWord)

{

u8 FMI_Timeout_Status=0;

u32 flashAddress;

FMI_WriteProtectionCmd(FlashSector, DISABLE);

FMI_EraseSector(FlashSector);

FMI_WaitForLastOperation(FMI_BANK_1);

flashAddress=FlashSector+Offset*2;

__asm

{

MOV R0, #0x00000

MCR p15,0x1,R0,c15,c1,0

}

// the following steps consume more then 500 ms....?

FMI_WriteHalfWord(flashAddress,*DataWord);

FMI_WaitForLastOperation(FMI_BANK_1);

}

Thanks in advance.

Satnam Singh

satnam
Associate II
Posted on May 17, 2011 at 09:59

i got the solution, just do a dummy sram read before checking the status flag.

Thanks.

myfirstadventure
Associate
Posted on May 17, 2011 at 09:59

The assembler code part should be added to the file ''STR91x.s''. All will be OK!

fred_blais5
Associate II
Posted on May 17, 2011 at 09:59

Hi, I'm trying to use the secondary flash as an ''emulated eeprom'' like in the application note but it does not work, I get errors like ''FMI_TIME_OUT_ERROR''. Someone has tips to access Bank1 and write some bytes to it?

satnam
Associate II
Posted on May 17, 2011 at 09:59

Hi fred,

Just try by using my code pasted above, remove the __asm codes and add a simple dummy sram read before

FMI_WaitForLastOperation(FMI_BANK_1);

Also ensure the scu clock for flash is enabled. my code works in secondary flash.

fred_blais5
Associate II
Posted on May 17, 2011 at 09:59

Forget about that, IT WORKS!!

Many thanks...

Why the f*** would we have to do that dummy read? Is it documented somewhere?

lloydepowell
Associate II
Posted on May 17, 2011 at 09:59

Yes, Fred. I also discovered by trial and error the need for a dummy Sram read. It is not documented. Also, the write 0xff to return to page read mode must be executed more than once to return to run operation.

Lloyd

fred_blais5
Associate II
Posted on May 17, 2011 at 09:59

Hey, thanks for answering me.

Can you give an exemple of a dummy sram read?

I don't get it... :-?