Skip to main content
dk5ug
Associate III
January 16, 2003
Question

Flash Update only?

  • January 16, 2003
  • 3 replies
  • 964 views
Posted on January 16, 2003 at 17:31

Flash Update only?

This topic has been closed for replies.

3 replies

dk5ug
dk5ugAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:53

Using the PSDsoft Express (v7.70) it looks as if the PLD is reconfigured

with every Flash update also. On the other hand I understand, PLD can

be reprogramed less often than Flash memory.

Is there a way to keep the PLD unchanged while updating Flash memory

only?

yu-jun
Associate
May 17, 2011
Posted on May 17, 2011 at 11:53

In Express software, when you do the last operatin: JATG/ISP, you can select Flash in 'PSD region ' part of step2 in dialogbox of JATG/ISP Operation. So that you can undate the Flash memory and keep other.

dk5ug
dk5ugAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 11:53

Thank you!

It works.

I feel better now.