cancel
Showing results for 
Search instead for 
Did you mean: 

External RAM 8 bits 64K Mux

jm
Associate II
Posted on July 25, 2003 at 09:26

External RAM 8 bits 64K Mux

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
jm
Associate II
Posted on July 25, 2003 at 08:58

Hi,

I don t understand something about external bus controler:

After configure correctly SALSEL=01 & CSSEL=01 register and BTYP=0; I use successful external RAM

But

when I want to use it in Mux mode (latch on POL), I change BTYP(=1) and it doesn t work. The signals seem good (CS1,RD,WR,Data&Adress) , but I can't neither write nor read the RAM (I verify data in Demux mode). After, I try to change wait state(0<=>15), no change......

So, if you have a suggestion, I will be happy !!

THANKS

maxime2399
Associate II
Posted on July 25, 2003 at 09:26

Beside an erroneous connection, I think you should verify the bus timings,

specially the timming related to the ALE/CS1 ALE/WR and ALE/RD.

look at the timing on the memory side and see if it fits in its specification.

If not, you may be able to update the configuration to make it work using the wait states, the tristate, changing the AEL length etc..