cancel
Showing results for 
Search instead for 
Did you mean: 

external interrupt 2

satnam
Associate II
Posted on July 02, 2009 at 02:46

external interrupt 2

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
bbalasa
Associate II
Posted on May 17, 2011 at 09:58

GPIO3 generates INT on EXTIT0_ITLine.(WIU group0 VIC1.10)

Use EXTIT0_ITLine instead of EXTIT2_ITLine

satnam
Associate II
Posted on May 17, 2011 at 09:58

Dear All,

I am trying to get external interrupt 2 on port pin 3.2 of MCU. I have done the following configuration but the code never enters the ISR section.

Also i have checked the configuration in simulator of KEIL, the VIC section shows that the group2 interrupt has been set, while i had set the extint2.

Please check the code and help me out with this problem.

/* Enable the GPIO3 */

SCU_APBPeriphClockConfig(__GPIO3, ENABLE);

SCU_APBPeriphReset(__GPIO3,DISABLE); /*out of RESET state*/

/* Enable WIU clock */

SCU_APBPeriphClockConfig(__WIU, ENABLE);

/* Enable VIC clock */

SCU_AHBPeriphClockConfig(__VIC,ENABLE);

SCU_AHBPeriphReset(__VIC,DISABLE); /* out of RESET state*/

// 3.2

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 ;//

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector;

GPIO_Init (GPIO3, &GPIO_InitStructure);

VIC_Config(EXTIT2_ITLine, VIC_IRQ,2);

VIC_ITCmd(EXTIT2_ITLine, ENABLE);

WIU_DeInit();

WIU_StructInit(&WIU_InitStruct);

WIU_InitStruct.WIU_TriggerEdge = WIU_FallingEdge;

WIU_InitStruct.WIU_Line = WIU_Line2;

WIU_Init(&WIU_InitStruct);

WIU_Cmd(ENABLE);

SCU_WakeUpLineConfig(2);

WIU_ClearITPendingBit(WIU_Line2);

WIU_ClearITPendingBit(2);

Other codes are also used for UART and RTC, they are working fine as interrupts.

Please ask if any more information or code is required.

Thanks and regards.

satnam
Associate II
Posted on May 17, 2011 at 09:58

Thanks for the help, now it is working.