cancel
Showing results for 
Search instead for 
Did you mean: 

Enquiry of availability of component for next 5 years as this will be used for New product design

ROOPA
Associate

Enquiry of availability of component for next 5 years as this will be used for New product design


P/N: SM5908 . Is this product can be used for New product design? OR is it NRND?

 

THANK YOU

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome @ROOPA to the community!

Despite its advanced age (the TVS SM5908 has been on the market since 1999), there are currently no signs of it being discontinued. The global market still needs to protect its products against overvoltage, for which TVS with 1500W are perfectly suited. As it is also the only TVS for 5V and such power, it will almost certainly still be available in 2029 and beyond. However, this is my personal assessment and we cannot provide a written guarantee.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @ROOPA to the community!

Despite its advanced age (the TVS SM5908 has been on the market since 1999), there are currently no signs of it being discontinued. The global market still needs to protect its products against overvoltage, for which TVS with 1500W are perfectly suited. As it is also the only TVS for 5V and such power, it will almost certainly still be available in 2029 and beyond. However, this is my personal assessment and we cannot provide a written guarantee.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.