cancel
Showing results for 
Search instead for 
Did you mean: 

download

cgerani9
Associate
Posted on July 26, 2009 at 15:22

download

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
cgerani9
Associate
Posted on July 26, 2009 at 15:22

Hi everyone,

I have just received a development board (ARM STM32F103) µ STM32F103RBT6

With this board, I received some examples. I try to download one of them by RS232 with the software ''Flash loader demo'' in version 1.3.

I use the project blinky (blinking led). I compile this with Keil µvision3

and this makes a file blinky.hex.

With this software of download, I reached to erase the component but at present, it's impossible to download this file ''blinky.hex'' due to a problem of address.

My parameters are :

Target : STM32F10xxBxx

PID (h) : 0410

version : 2.1

All addresses are Unprotected

next

On one screen

Download to device :

c:\Keil\ARM\Examples\Obj\Blinky.hex

(the adress information is just in read mode)

next

Target : STM32F10xxBxx

Mapfile : STM32F10xxBxx.STmap

Opretaion : ERASE

File name : c:\Keil\ARM\Examples\Obj\Blinky.hex

File size : 128Kb (it's very strange because the capacity of this file

is only 1581 bytes on the hard disk)

And the error message is : FAIL : Address not allowed

Thank you very much for your help

null