cancel
Showing results for 
Search instead for 
Did you mean: 

DMA Controller

petera.stephens9
Associate II
Posted on April 25, 2005 at 15:50

DMA Controller

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
petera.stephens9
Associate II
Posted on April 15, 2005 at 20:39

Do the STR7 series parts have a DMA controller or equivalent? It probably does and I just missed it, but I don't see it in the documentation for the part.

hichem2
Associate II
Posted on April 18, 2005 at 06:38

Hello,

In the STR7xx family, for the moment we have already STR720 support a DMA controller.

The DMA controller provides access to 2 data streams inside STR720 system, each data stream can be associated to one particular peripheral, which triggers a DMA request starting the data transfer between the corresponding buffers defined in the stream descriptor.

Hope that this can Help you

Hich, :p

petera.stephens9
Associate II
Posted on April 18, 2005 at 13:58

So the STR71x parts do not have DMA support?

hichem2
Associate II
Posted on April 19, 2005 at 05:24

Hi Delphi_Pete,

Sorry, as I said for the moment only the STR71x support a DMAC but also we have STR730 product which will be available on the market soon, it support a DMAController.

For more information concerning the STR7xx family you can see:

http://mcu.st.com/modules.php?name=mcu&file=pfinder&FAM=ARM7

Cheers,

Hich :p

hichem2
Associate II
Posted on April 25, 2005 at 15:50

Hello,

STR73x family is not published yet, but the STR73x package will be available soon and then you can find all the peripherals characteristic in the reference manual which will be available on the web page.

Thank you for your comprehension.

Cheers,

Hich ;)