2011-11-25 5:45 AM
I would like to use DMA with SSP1. There is a problem that when flow control is set to peripheral, data are transfered, but I am not able to control how many bytes are transfered. If I change flow control to DMA, nothing happens. Any single transfer doesn't occur, although both single and burst requests are signaled (registers DMA_SSBR and DMA_SBRR).
I can't find where is the error. I believe I did my best according to documentation. In previous topics there was an example (Example of DMA and SSP, 11/9/2006 2:10 AM), but the attachment is lost and no longer available. Eris, can you post it again? Tomas My code: ============================================================== #define SPI_SD SSP1 #define DMA_CHANNEL_RX DMA_Channel4 #define DMA_CHANNEL_TX DMA_Channel5 #define DMA_CHANNEL_RX_IDX Channel4 void str91_dma_transfer_receive( const BYTE *buff, UINT count) { DMA_InitTypeDef DMA_InitStructure; WORD rw_workbyte[] = { 0xffff }; DMA_DeInit(); DMA_Cmd(ENABLE); // shared DMA configuration values DMA_InitStructure.DMA_Channel_LLstItm = 0; DMA_InitStructure.DMA_Channel_DesWidth = DMA_DesWidth_Byte; DMA_InitStructure.DMA_Channel_SrcWidth = DMA_SrcWidth_Byte; DMA_InitStructure.DMA_Channel_DesBstSize = DMA_DesBst_1Data; DMA_InitStructure.DMA_Channel_SrcBstSize = DMA_SrcBst_1Data; DMA_InitStructure.DMA_Channel_TrsfSize = count; // RX - storing data in buffer DMA_InitStructure.DMA_Channel_SrcAdd = (DWORD)(&SPI_SD->DR); DMA_InitStructure.DMA_Channel_DesAdd = (DWORD)buff; // DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl2_DMA; // peripheral_to_memory / DMA DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl_Perip2; // peripheral_to_memory / SSP DMA_InitStructure.DMA_Channel_Src = DMA_SRC_SSP1_RX; DMA_InitStructure.DMA_Channel_Des = 0; DMA_Init(DMA_CHANNEL_RX, &DMA_InitStructure); DMA_ChannelSRCIncConfig(DMA_CHANNEL_RX, DISABLE); DMA_ChannelDESIncConfig(DMA_CHANNEL_RX, ENABLE); // TX - must send 0xFF DMA_InitStructure.DMA_Channel_SrcAdd = (DWORD)rw_workbyte; DMA_InitStructure.DMA_Channel_DesAdd = (DWORD)(&SPI_SD->DR); // DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl1_DMA; // memory_to_peripheral / DMA DMA_InitStructure.DMA_Channel_FlowCntrl = DMA_FlowCntrl_Perip1; // memory_to_peripheral / SSP DMA_InitStructure.DMA_Channel_Src = 0; DMA_InitStructure.DMA_Channel_Des = DMA_DES_SSP1_TX; DMA_Init(DMA_CHANNEL_TX, &DMA_InitStructure); DMA_ChannelSRCIncConfig(DMA_CHANNEL_TX, DISABLE); DMA_ChannelDESIncConfig(DMA_CHANNEL_TX, DISABLE); // reusing the same data in memory // enable interrupts DMA_ITConfig(DMA_CHANNEL_RX, ENABLE); DMA_ITConfig(DMA_CHANNEL_TX, ENABLE); DMA_ITMaskConfig(DMA_CHANNEL_RX, DMA_ITMask_ITC, ENABLE); DMA_ITMaskConfig(DMA_CHANNEL_TX, DMA_ITMask_ITC, ENABLE); // Enable TX/RX request in SSP controller SSP_DMACmd(SPI_SD, SSP_DMA_Receive, ENABLE); SSP_DMACmd(SPI_SD, SSP_DMA_Transmit, ENABLE); // Enable DMA channels DMA_ChannelCmd(DMA_CHANNEL_RX, ENABLE); DMA_ChannelCmd(DMA_CHANNEL_TX, ENABLE); // wait for end of transfer while (DMA_GetITStatus(DMA_CHANNEL_RX_IDX, DMA_TCRS) == RESET); // Disable DMA channels DMA_ChannelCmd(DMA_CHANNEL_RX, DISABLE); DMA_ChannelCmd(DMA_CHANNEL_TX, DISABLE); // Disable TX/RX request in SSP controller SSP_DMACmd(SPI_SD, SSP_DMA_Transmit, DISABLE); SSP_DMACmd(SPI_SD, SSP_DMA_Receive, DISABLE); DMA_Cmd(DISABLE); } // str91_dma_transfer_receive2018-08-10 4:14 PM
I am having this issue also. Im using a STR911FAx44. I know this post is old but I would like to see an asnwer. I am in the process of updating legacy firmware and would like to use the DMA. Interrupt does not fire until, what looks like the entire ram space is transferred. I am transferring to the UART in my case.