cancel
Showing results for 
Search instead for 
Did you mean: 

Correct setting for internal flash

alexanderpapsdorf9
Associate II
Posted on July 09, 2009 at 12:29

Correct setting for internal flash

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
alexanderpapsdorf9
Associate II
Posted on May 17, 2011 at 09:59

Hello,

I have a question concerning the flash configuration. In the most examples from ST, the FMI clock is set to 96 MHz and the Flash is configured with the following settings.

FMI_Config(FMI_READ_WAIT_STATE_2, FMI_WRITE_WAIT_STATE_0, FMI_PWD_ENABLE, FMI_LVD_ENABLE, FMI_FREQ_HIGH);

According to the STR912FA manual, the FMI clock can be set to 96 MHz if the flash size is <= 512 KB. But what is the right number of read wait states?

In the datasheet of the STR912FA is written on page 69 the follwing note :

 

Note: Flash read access for sequential addresses is 0 wait states at 96 MHz. Flash read access

 

for non-sequential accesses requires 2 wait states when FMI clock is above 66 MHz. See

 

STR91xF Flash Programming Manual for more information.

 

In the STR91xFA Flash programming manual on page 32 for Flash configuration you can find the following note :

 

Note: Wait States are inserted only for non-bursting Flash read bus cycles. One

 

wait state is required for a FMI bus clock frequency of 66 MHz or less. Two wait

 

states are required for 75 MHz bus clock frequency.

 

What is now the correct setting? Two wait states (according to the datasheet) or 3 wait states (according Flash manual)?

King regards

Alex