cancel
Showing results for 
Search instead for 
Did you mean: 

Code banking

jrajeev
Associate II
Posted on February 08, 2006 at 10:57

Code banking

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jrajeev
Associate II
Posted on May 17, 2011 at 12:10

We are working on ST upsd3334DV on DK3300 development kit. We are facing problems in the genertion of *.hex,*.obj files when the Code banking is selected in the options for the target. We request you to send the procedure for the above requirement.

IDE Keil uVision V8.0

Code size more than 64K

RAM size requirement More than 8K so need to configure the secondary flash