2008-04-28 5:31 AM
2011-05-17 12:52 AM
Help!
I am trying to configure the serial port 0 to function at different baud rates. The port is functioning, however when I change the baud rate it only prints 0. The first stream at 9600 is correct. I then step up the baud rate to 19200, 38400, etc. Only 9600 works. If I init the port to 19200 then only 19200 works. This seems a bit buggy to me. Anyone had the same issues - or can anyone help me out here? Regards Quentin