2021-11-08 8:22 AM
Hello ST,
I’m attempting to integrate the STEVAL-STRKT01 into my system.
I need to issue NMEA commands to the Teseo .
I’m connected into the UART over CN503 (TX,RX,GND only) and I can see the serial chatter.
For example, I want to Stop the STAGPS engine with $PSTMSTAGPSONOFF,0*4A
This, and all other commands I am testing, are getting no responses. Am I doing something wrong, or can I not send NMEA to the Teseo on this Evaluation board?
Attached a screenshot of one of the billion ways I’ve tried this. Any help much appreciated!
2021-11-08 9:26 AM
How about a simpler firmware version query?
Any inbound commands work?
TESEO-SUITE ?
2021-11-08 1:28 PM
Its hard to tell if my NMEA commands are triggering any response at all, the UART is sporadically spooling out NMEA messages info without being prompted. Including versioning info.
I suspect the STEVAL-STRKT01 board is continuously interrogating the Teseo and has exclusive use?
I set up the Teseo-suite, image attached, but still couldn't get it to accept PSTMSTAGPSONOFF..
2021-11-09 8:47 AM
After exhaustive testing, no. No inbound commands are being accepted by the STEVAL-STRKT01's onboard Teseo. I reckon its just how this evaluation board is set up.. I'd love to find a safe way around this!
2021-11-09 9:47 AM
Would check you're not getting some conflicting signals on the GPS's RX pin from the LoRa MCU, or other sources/connections.
https://www.st.com/resource/en/schematic_pack/steval-strkt01_schematic.pdf
2021-11-09 10:46 AM
Thanks for your analysis - that's almost certainly right. The Lora module does seem to be obstructing my commands.
Do you think I can hope to interrupt (temporarily) this UART connection between LoRa & LIV3 without damaging the hardware? I don't see an obvious move here..
2021-11-09 11:00 AM
I'd probably start by removing resistor/zero-ohm R204, so you can connect via TP202
2021-11-09 12:13 PM
I see , yes. Ok, I'll let you know how it works.
Thanks a mil!