cancel
Showing results for 
Search instead for 
Did you mean: 

Bugs in STR71x software library

per239955_st
Associate II
Posted on February 15, 2005 at 10:37

Bugs in STR71x software library

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
per239955_st
Associate II
Posted on February 02, 2005 at 12:48

Hi,

I would like to report 2 bugs in the STR71x software library.

Both are in the BSPI module.

void BSPI_ClkFEdge(BSPI_TypeDef *BSPIx, FunctionalState NewState)

is ''inverted''. When setting it to ENABLE it gets DISABLEd and vice versa.

FlasgStatus BSPI_FlagStatus(BSPI_TypeDef *BSPIx, BSPI_Flags flag)

doesn't reurn the correct value. (because of a faulty equal sign in the function)

Are there any list of known bugs in the library?

Regards

/Beach/

PS.

I must say that I like this 'simple' lib.

Grouping all registers of a hardware module into a structure makes the code very nice looking. :D

DS.

technischesoftware
Associate II
Posted on February 04, 2005 at 16:41

Hi,

thanks.

This clarifies the problem I had with a MMC card connected via the BSPI. Due to the reported bug a read followed by a write access occurs. If between both accesses the BSPI changes the addressed flag then the write operation can corrupt this flag.

Regards

per239955_st
Associate II
Posted on February 07, 2005 at 06:57

Found another ''bug''.

In the file tim.h the line

#define TIM_OCBIE_mask 0x0080

should be

#define TIM_OCBIE_mask 0x0800

/Beach

hichem2
Associate II
Posted on February 07, 2005 at 09:59

Hello Beach,

You are right this is a STR71x BSPI library mistake and it will be corrected in the next release.

Thank you and best regards

Hich :p

[ This message was edited by: Hich on 07-02-2005 14:30 ]

per239955_st
Associate II
Posted on February 07, 2005 at 13:16

Yet another bug in the BSPI module.

void BSPI_TrFifoDepth(BSPI_TypeDef *BSPIx, u8 TDepth)

and

void BSPI_RcFifoDepth(BSPI_TypeDef *BSPIx, u8 TDepth)

should accept depth values 1-10, but will only accept 1-9.

10 will set the depth to 1.

/Beach

hichem2
Associate II
Posted on February 09, 2005 at 05:08

Hello Beach,

Thank you,I think you can be a best approver ;)

All your comments will be corrected in the next release.

With regards,

Hich :p

e239955_stm1_stmicro
Associate II
Posted on February 14, 2005 at 11:08

Hi,

I found also a bug in the flash library in the function :

void FLASH_FlagClear(flashflags Xflag)

When for example, you have :

FLASH_FlagStatus(FLASH_BSY0) in the WaitForLastTask(flashbanks Xbank) function.

FLASH_BSY0 = 0x21;

So the TempReg variable is egal to 1. So the case value for CR0 register should be ''1'' and not the ''0'', and so on ...

The Lock bit in FLASH_CR0 register is not tested, it should also be tested ???

Why do I need to make a wait loop to wait the end of the write to flash execution. When the Lock bit is set all the flash is blocked, when it's released then I could write another byte, and so on...

Best regards

OneR

hichem2
Associate II
Posted on February 15, 2005 at 10:37

Hello OneR,

Yes you are right, but this bug is already detected and corrected in the V2.0, it will be published soon.

With regards,

Hich. :p