cancel
Showing results for 
Search instead for 
Did you mean: 

BIOS flash write doesn't seem to work on Elite eval board

peterfox9
Associate II
Posted on November 05, 2003 at 11:03

BIOS flash write doesn't seem to work on Elite eval board

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
peterfox9
Associate II
Posted on November 05, 2003 at 07:43

I'm having trouble writing to the BIOS flash on the development board.

I use

mio m8 ffff0000 0

but don't see any write strobes on the Bios flash device.

Even after using

mio dx8 22 51 4

to enable ROM writes,

mio m8 ffff0000 0

doesn't result in any write strobes.

Reading the bios works fine.

This is on the Elite development board, running linux (Redhat 7.1).

Have I missed something ?

Replying to myself - yes !

I've modified the linuxbios flash_rom program to

continuously do the flash ident accesses.

This is write, write, write, read, read, write in a loop.

MEMWR is busy with no gaps,

MEMRD has nothing (except for the refresh cycles).

Perhaps it is a shadowing problem ?

[ This message was edited by: pjhf on 05-11-2003 12:46 ]
peterfox9
Associate II
Posted on November 05, 2003 at 11:03

It's a bug in the freebios code I was using to access the flash.

A missing volatile allowed the C compiler to reorder the flash

accesses so that the ident wasn't read properly.