cancel
Showing results for 
Search instead for 
Did you mean: 

arm jtag interface.

ongth60
Associate II
Posted on August 09, 2005 at 02:00

arm jtag interface.

This discussion is locked. Please start a new topic to ask your question.
16 REPLIES 16
ongth60
Associate II
Posted on July 08, 2005 at 01:33

Hi,

My fabricated main board that contains the ARM cpu could worked well with the JTAG board from the evaluation board. I soldered some wires from the JTAG port of the evaluation board to my fabricated main board which contains the ARM cpu. The link is robust and I can connect and disconnect at every instance.

The reason I'm using this method is that I can't get a robust link with another JTAG board which I have constructed based on the schematics(debug1.jpg and debug2.jpg) posted above. JTAG board constructed based on debug1.jpg schematic can work but the link is not robust enough. It can connect only 3 times out of 10 times), so I've decided to construct the other JTAG board which contains the reset circuitry based on debug2.jpg.(Pls note that I've changed the transistors) By then, it could nt work well and the errors that I've got are stated above.

So, now I've tried to test with a workable evaluation board but my emulator refuse to cooperate.

rgrds,

ongth60

ongth60
Associate II
Posted on July 08, 2005 at 05:24

Hi ibtiss,

Thanks for ur support.

1.I've tried rebooting the PC before running the RVD and the same problem still occurs.

2.The second option is how do i run armcc from command line?

Pls advise.

Rgrds,

ongth60

ongth60
Associate II
Posted on July 08, 2005 at 07:23

Hi,

Ive got the below:

Microsoft Windows XP [Version 5.1.2600]

(C) Copyright 1985-2001 Microsoft Corp.

C:\Documents and Settings\Jim>armcc

ARM/Thumb C/C++ Compiler, RVCT2.0.1 [Build 313] for ST [basic for ARM7]

Usage: armcc [options] file1 file2 ... filen

Main options:

--arm Generate ARM code

--thumb Generate Thumb code

--c90 Switch to C mode (default for .c files)

-O0 Minimum optimization

-O1 Restricted optimization for debugging

-O2 Maximum optimization

-Ospace Optimize for codesize

-Otime Optimize for maximum performance

--cpu Select CPU to generate code for (eg. ARM9E/ARM10E)

-o Name the final output file of the compilation

-c Compile only, do not link

--asm Output assembly code as well as object code

-S Output assembly code instead of object code

-fs Interleave source with disassembly (use with -asm or -S)

-E Preprocess the C source code only

-D Define on entry to the compiler

-g Generate tables for high-level debugging

-I Include on the #include search path

For support please contact your tools supplier

Software supplied by: ARM Limited

License is dongled to RVI-ME

C:\Documents and Settings\Jim>

Err, what is the command syntax to connect RVI-ME via DOS?

rgrds,

ongth60

ongth60
Associate II
Posted on July 08, 2005 at 08:07

Hi,

I've tried the autoconfigure scan chain

Respond was:

Error:Auto configure failed.

Check the RVI connection with the target or try using a lower fixed frequency.

rgrds,

ongth60

ongth60
Associate II
Posted on July 10, 2005 at 04:48

Hi ibtiss,

i dun have an example in the onchip flash memory, therefore I can't confrim with you whether the RVIME is broken or not. However, I have probed the signals of JTAG with J4 jumper not fitted:

Signals of JTAG when not connected to emulator:

Pin 1 - 3.29V

Pin 2 - 3.29V

Pin 3 - 3.29V

Pin 4 - ground

Pin 5 - 3.29V

Pin 6 - ground

Pin 7 - 3.29V

Pin 8 - ground

Pin 9 - 3.29V

Pin 10 - ground

Pin 11 - ground

Pin 12 - ground

Pin 13 - 1.230V

Pin 14 - ground

Pin 15 - 2.83V

Pin 16 - ground

Pin 17 - 0V

Pin 18 - ground

Pin 19 - 0V

Pin 20 - ground

Signals of JTAG when connected to emulator:

Pin 1 - 3.29V

Pin 2 - 3.29V

Pin 3 - 0.016V

Pin 4 - ground

Pin 5 - 0.981V

Pin 6 - ground

Pin 7 - 0.978V

Pin 8 - ground

Pin 9 - 0.971V

Pin 10 - ground

Pin 11 - ground

Pin 12 - ground

Pin 13 - 0.374V

Pin 14 - ground

Pin 15 - 0.115V

Pin 16 - ground

Pin 17 - 0V

Pin 18 - ground

Pin 19 - 0V

Pin 20 - ground

Pls advise.

Rgrds,

ongth60

[ This message was edited by: ongth60 on 10-07-2005 09:40 ]

ongth60
Associate II
Posted on July 14, 2005 at 05:59

Hi,

anyone can help me to troubleshoot the problem cos to get a new emulator will take me 6 weeks.

Rgrds,

ongth60

ongth60
Associate II
Posted on August 09, 2005 at 02:00

Hi ibtiss,

Ya, got my replacement and indeed the emulator was spoilt. Thanks for looking up into it.

Rgrds,

ongth60