2003-07-29 12:51 AM
About ST90158M9,Would you like to help me please?
2011-05-17 2:34 AM
I get troubles with the microcontroller ST90158M9.
Where could I get the C compiler with the ST90158M9? And how do I use these tools? thanks your kindly help!2011-05-17 2:34 AM
On Internet
you should be able to download the following SW: ST9 V6.1.8 Toolchain R6.1.8 Apr-2003 17109KB This toolchain contains a C compiler for ST9, the ST9 Assembler-Linker and an integrated development environment, ST9 Visual Debug which provides the host interface for ST9 emulators (see below). This toolchain should be used if you are working with General Purpose MCUs (ST90158 - ST92F12X - ST92141 - ST92163 - ST92F150 - ST92F250). This release supports the ST92F150-EMU2 and contains the downloader utility for upgrading/reconfiguring most ST9 HDS2V2 emulators.