cancel
Showing results for 
Search instead for 
Did you mean: 

VNH3SP30-E

rcolman
Associate
Posted on October 11, 2012 at 15:00

I would like to use a VNH3SP30-E to control the rotation of a dc motor. No PWM. My question is about the inputs, INA, INB, ENA and ENB. Do I need pullup and/or series resistors for these inputs? Can I just tie the ENA and ENB to +5V? The inputs INA and INB will be either +5V or gnd.

1 REPLY 1
Posted on October 12, 2012 at 16:27

Dear Customer,

We recommend to insert the pull-up/series resistors as stated in the application schematic inserted in the datasheet (fig.33):

-

         

ENx: 3.3K for Pull-up resistor;

-

         

INx: 1K as series resistor; 

We are available for any further information you may need. 

Best Regards,

Rosario Ruggeri

STMicroelectronics