cancel
Showing results for 
Search instead for 
Did you mean: 

Could you please recommend ST's drop in replacements for following ICs?

JZhen.7
Associate

ONSEMI MPN

NC7WZ16P6X

NL27WZ16DFT2G

 NC7SZ74K8X

NL17SZ74USG

NLV17SZ74USG

NC7SZ125P5X

NL17SZ125DFT2G

NC7SZ74K8X

NC7SZ27P6X, SN74LVC1G27DCKR

1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Welcome, @JZhen.7​, to the community!

For many years, ST has only had this type of logic devices in its range for space applications, so it does not offer any drop-in repacements for industrial applications. But you can check the automotive section, if their pricing is acceptable for you.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Welcome, @JZhen.7​, to the community!

For many years, ST has only had this type of logic devices in its range for space applications, so it does not offer any drop-in repacements for industrial applications. But you can check the automotive section, if their pricing is acceptable for you.

Good luck!

If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
JZhen.7
Associate

Thank you very much.