Other: software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Accelrometer/gyro (LSM6DS3TR-C) Test

Hi ,Working on LSM6DS3TR-C sensor.acceleraotmeter /gyro not able to generate the perfect values . please help me how to get the exact values . may i know what is the mounting matrix for this sensor ?i have configured in dts as below ,i2c0 {pinctrl-na...

nareshnakka_0-1702992887175.png nareshnakka_0-1702993270827.png

eDesignSuite

High all,This  Application (eDesignSuite) does not start in the browser, only empty window with rotating circle.I am logged in and would like to make a design (isolated flyback).Operating system is Windows 10, Browsers are Firefox 115.7.0.esr or MS E...

İnstallation of STM32

Hello.I am trying to install the program but it gives an error. I can't get past step 7. In step 7, the quit option appears. I tried it on 5 different computers. always the same error. what could be the reason for this? Please help me.

Bcanbaz by Associate
  • 834 Views
  • 1 replies
  • 0 kudos

Resolved! ST website bad gateway error

Hello,    I can not login to ST website. I was trying to download the Unicleo-GUI. Each time I try, when I press on the "user" icon from the main st.com page, a "bad gateway" error message is shown. In the past I was able to login.  EDIT: A day after...

MRaff.1 by Associate III
  • 820 Views
  • 1 replies
  • 0 kudos

HVLED101 adding transformer

In the HVLED101 design tool, there is the option for a custom transformer. When selecting the core type it seems possible to add a new core type (component) for a transformer design. When adding one, a screen pops up that says "Please, compile the fo...

Johnno by Associate II
  • 1493 Views
  • 6 replies
  • 2 kudos

eDsim

Hello, i would like to simulate a schematic of a 100W USB PD adapter that include the STUSB4761 usb pd controller using eDsim but i can’t find the controller in the library can any one help me please.

nesrine12 by Associate III
  • 5314 Views
  • 1 replies
  • 0 kudos

L6470

Hi,I am usinga) L6470 to control Stepper motors. I am using STP-MTR-23079(x). The motor has rated current=2.8A/phase, Resisteance=1.1ohm/phase.b) I am using 24VDC for L6470.c) I am setting KVAL = 14.04% with phase current that is around 3.07A/phase. ...

CSu.12 by Associate II
  • 539 Views
  • 0 replies
  • 0 kudos